Limit the impact of the fault within the installation

In the event of a fault, the voltage of the installation is severely affected and risks causing a loss of loads. In particular the management of faults related to short circuits within a critical installation using static transfer systems (STS) is particularly important.

In order to guarantee the continuity of the supply to their load, the STS must:

  • Operate autonomously
  • Be able to detect and differentiate a short-circuit downstream or upstream
  • Carry out a transfer of sources without overlap to avoid the propagation of the fault
  • Ensure the islanding of a short-circuited load

In the event of a short-circuit downstream of an STS, it must isolate the fault to prevent its propagation and alert the operator. The other STS connected to the same source must protect their load by immediately transferring it to an alternative source without propagating the fault.

Continuity
ANALYZE THE FAULT
BEFORE TRANSFER
Islanding
DO NOT PROPAGATE
THE FAULT
Example of a 2N installation

 

Case of a fault downstream of the STS

1 - Short-circuit on a load

Image
Promesse_27_schem_030_a_gb_0.jpg

A short-circuit appears on a load supplied by source B and induces a voltage disturbance on the distribution of source B.

2 - Islanding of the faulty load

Image
Promesse_27_schem_031_a_gb_0.jpg

The local STS isolates the fault on source B by preventing its transfer. The other STS immediately transfer their load to source A without overlap.

3 - Loads protection

Image
Promesse_27_schem_032_a_gb_0.jpg

The fault has been isolated on source B and the other loads are protected by source A.

 

 

Legend

Promesse_27_schem_033_a_gb_1.jpg

 

 

Case of a fault upstream of the STS

For a fault upstream of the STS the fault isolation strategy consists of transferring all the loads to the healthy source without overlapping the sources.

1 - Fault upstream of the STS

Image
Promesse_27_schem_034_a_gb_1.jpg

A fault occurs upstream of an STS supplied by source B causing a voltage disturbance on the distribution of source B.

2 - Transfer of loads to the healthy source

Image
Promesse_27_schem_035_a_gb_1.jpg

The STS immediately transfer their load to source A without overlap.

3 - Loads protected

Image
Promesse_27_schem_036_a_gb_1.jpg

The fault has been isolated on source B and the other loads are protected by source A.

Socomec solution

STATYS static transfer systems

The STATYS range of static transfer systems (STS) incorporates in its design more than 30 years of experience and 4 generations of STS. The thousands of hours of operation and the many units installed have improved the detection and qualification of faults. It maximizes availability by guaranteeing transfer without overlap as well as fault isolation in the event of a downstream short-circuit.