Shutdown clients for virtual machine infrastructures using MicrosoftTM Hyper-V, VMware® or CITRIX XenServer operating system
If a UPS is being used to supply power to Host and Clusters it can be configured to respond to critical conditions by bringing about a controlled shutdown of the entire virtual infrastructure. With the UPS connected to the LAN, the VIRTUAL JNC shutdown client can be installed on the infrastructure in a single operation.
VIRTUAL JNC is compatible with the following network interfaces:
- Net Vision
- RT Vision
Service Forms and personalization of communications must be enabled.