Spare power module available 24/7 on customer site
The addition of the Power module as a spare option to the maintenance contract of MODULYS XL will always allow to maintain the level of availability of the installation.
A spare power module will be to hand next to the MODULYS XL so that the module can be swapped in case of failure in less than 5 minutes.
Continuous availability
The spare power module & maintenance station are available 24/7 at the customer's site.
The power module can be replaced in online mode in less than 5 minutes.
Low MTTR
The power module can be replaced quickly by the customer: no wiring, no computer and no software.
Software alignment is automatic.
The replacement power module is "ready to use", complete, always operational and tested.
All inclusive
The price is “all inclusive” and comprises:
- a maintenance slot and a spare power module rental,
- training to enable the customer to change the module by himself and avoid any problems,
- the maintenance of the spare module (spare parts and consumables).